USB camera not detected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB camera not detected

2,353 Views
johnjacobjohn
Contributor I

Hi,

   I am currently using the SABRE AI board with the BCM89810 phy card. The card is getting detected and I am able to stream from the board to a PC(using a technica converter) using gstreamer. But when I try to connect a USB camera, the camera is not getting detected in /dev. This happened only after applying the patches for BCM89810. It worked fine in the kernel in which the patch was not applied. How can we detect the usb camera with the new kernel (after applying bcm patch).

Thank you,

John Jacob 

Tags (2)
0 Kudos
Reply
1 Reply

2,192 Views
igorpadykov
NXP Employee
NXP Employee

Hi John

usb has some limitations on sabre ai board, please check attached Release

Notes Table 16. Known issues and workarounds for i.MX 6Dual/6Quad SABRE-AI for usb issues.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply