USB audio and video class support for the i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB audio and video class support for the i.MX6

1,528 Views
Larry5335
Contributor IV

Does the i.MX6 with the 3.0 Linux kernel support both the USB Video and Audio classes?

UVC and UAC?


Tags (2)
0 Kudos
Reply
2 Replies

1,197 Views
Yuri
NXP Employee
NXP Employee

According to Table 5 (Supported Features) of "i.MX_6Solo6DualLite_SABRE-AI_Linux_Release_Notes.pdf" (L3.0.35_4.1.0) :
USB (Host mode) supports : MSC, HID, UVC, USB audio.

0 Kudos
Reply

1,197 Views
YixingKong
Senior Contributor IV

Larry

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the issue, can we close the discussion? If you still need Freescale help, please feel free to contact us.

Thanks,

Yixing

0 Kudos
Reply