USB WiFi dongles

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB WiFi dongles

1,817件の閲覧回数
PeteSwenson
Contributor I

Has anyone tested or know of any working USB WiFi dongles with the QSB?  There appears to be support for Atheros, but I don't know to what extent.

 

I've plugged in the following, but they didn't come up:

 

Linksys WUSB300N

Rosewill RNX-G1

TP-LINK TL-WN321G

 

Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,622件の閲覧回数
CraigPetku
Contributor III

I enabled the dlink DWA-160A2 (under $20 on ebay) under Android a couple weeks back on an EVK derivative.  Should work on the QSB as well.  The biggest trick is WPA supplicant.  If I have some time I'll try to post a clean patch for the QSB Ubuntu as well, but you may find the attached a little helpful.  The driver is compiled as a .ko as part of the kernel build then manually copied to a prebuilt folder along with the firmware files.

0 件の賞賛
返信