USB Test Packets for USB-IF Compliance Testing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Test Packets for USB-IF Compliance Testing

2,499件の閲覧回数
joshk
Contributor I

Hello,

     I just wanted some clarification on how the Test Packets are generated for USB Compliance testing (USB 2.0 Specifications 7.1.20) for a device (IE the IMX6-SL is the Device).   From what I gathered the controller sends the test packets so I would like to confirm that I do not need to write the any code to create and send this test packet?

Thank you!

Josh

ラベル(2)
0 件の賞賛
返信
1 返信

2,158件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Josh

for description of setting usb test modes one can look at

sect.34.10 Testing the device mode  iMX6_Firmware_Guide.pdf

included in i.MX 6Series Platform SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信