USB_OTG1 power clarification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB_OTG1 power clarification

1,260 Views
NIKHITHAANTONY
Contributor I

In the schematics designed using I.MX7 processor, USB type c connector is used for charging and data transfer. But which power will be connected to the OTG1_VBUS pin. USB power can't be connected since USB will get power only at the time of charging and during data transfer USB will not get power. And also there is 5v output from the PMIC, that also can't connect directly, since when our circuit is powered up, USB will get power all the time.

So what is the best method for giving power to the USB_OTG1, so that it will get powered only if dp and dn of OTG1 signals are used.

0 Kudos
Reply
1 Reply

1,256 Views
igorpadykov
NXP Employee
NXP Employee

Hi NIKHITHA

 

VBUS is described in Table 12. USB recommendations  Hardware Development Guide for i.MX7Dual and 7Solo Applications Processors

"The processor should turn VBUS on as required."

Solution can be found in Sabre SD schematic SPF-28590 p.7,21  Design files for i.MX 7Dual

 

Best regards
igor

0 Kudos
Reply