USB Host in IMX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Host in IMX6UL

2,356 Views
chandraevolute
Contributor V

I have a I.MX6UL custom board, we are using one OTG port as Host with ID pin configured to charge the Android tablet connected to that port. Here my Android Tab USB acts like Device and IMX6UL usb port acts as Host. So i have emulated the USB as gadget serial and I am able to communicate to a Ubuntu machine via Serial read and write. 

Now I have to do the same thing with Android tab connected to IMX6UL board. Both charging and communication should happen as a Virtual com?

Labels (3)
Tags (1)
0 Kudos
Reply
2 Replies

2,139 Views
igorpadykov
NXP Employee
NXP Employee

Hi chandra

>Now I have to do the same thing with Android tab connected to IMX6UL board.

>Both charging and communication should happen as a Virtual com?

I believe the same configuration is also possible, Android tablet acting as host and IMX6UL board

as USB Device configured as CDC. If both Android and IMX6UL board support charging

this is also feasible option.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,139 Views
chandraevolute
Contributor V

Thank you igor,

I will get back to you once the android application is done

0 Kudos
Reply