USB Host in IMX6UL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB Host in IMX6UL

2,348 次查看
chandraevolute
Contributor V

I have a I.MX6UL custom board, we are using one OTG port as Host with ID pin configured to charge the Android tablet connected to that port. Here my Android Tab USB acts like Device and IMX6UL usb port acts as Host. So i have emulated the USB as gadget serial and I am able to communicate to a Ubuntu machine via Serial read and write. 

Now I have to do the same thing with Android tab connected to IMX6UL board. Both charging and communication should happen as a Virtual com?

标签 (3)
标记 (1)
0 项奖励
回复
2 回复数

2,131 次查看
igorpadykov
NXP Employee
NXP Employee

Hi chandra

>Now I have to do the same thing with Android tab connected to IMX6UL board.

>Both charging and communication should happen as a Virtual com?

I believe the same configuration is also possible, Android tablet acting as host and IMX6UL board

as USB Device configured as CDC. If both Android and IMX6UL board support charging

this is also feasible option.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,131 次查看
chandraevolute
Contributor V

Thank you igor,

I will get back to you once the android application is done

0 项奖励
回复