USB Camera Not Working on IMx8QM MEK Android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Camera Not Working on IMx8QM MEK Android

4,380 Views
ajmalmali
Contributor II

Hi

I am trying to develop some Camera application in iMx8QM MEK running Android Q.

I am using "Logitech C270 HD WEBCAM" for my application.

In the MEK, I have observed that the default camera application is not working. PFA the logs

 

My initial requirement is to develop a sample Android camera application that uses external USB camera as the input.

The app should be able to detect the USB camera as the default camera option using camera2 API.

 

Is there any configuration to be done to enable USB camera in iMx8QM MEK with Android 10?

 

Regards

Ajmal

0 Kudos
Reply
1 Reply

4,333 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport
0 Kudos
Reply