USB Camera Not Working on IMx8QM MEK Android

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Camera Not Working on IMx8QM MEK Android

4,273件の閲覧回数
ajmalmali
Contributor II

Hi

I am trying to develop some Camera application in iMx8QM MEK running Android Q.

I am using "Logitech C270 HD WEBCAM" for my application.

In the MEK, I have observed that the default camera application is not working. PFA the logs

 

My initial requirement is to develop a sample Android camera application that uses external USB camera as the input.

The app should be able to detect the USB camera as the default camera option using camera2 API.

 

Is there any configuration to be done to enable USB camera in iMx8QM MEK with Android 10?

 

Regards

Ajmal

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 返信

4,226件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信