UM805RE on the IMXUL 9x9 Ref design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UM805RE on the IMXUL 9x9 Ref design

2,279件の閲覧回数
kaveeh
Contributor I

Hello,

What is the purpose of using U708 in the IMX6UL 9x9 Ref design?

I guess the external LDO U701 is also used to power-up the U708 from off mode. So, if we remove the U708 and populate the R758 then is it possible as well to remove the external LDO (U701).

Thanks,

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,026件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Kaveh,

I understand,  please create a  CASE,  using our  web page  http://nxp.com/support and click under the Hardware & Software, we can continue the discussion in private using that platform.

0 件の賞賛
返信

1,025件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Kaveh,

Can you share the schematics that you are mention,  NXP only offers the i.MX6UL EVK board.  which does not use the 9x9 i.Mx6U device.

0 件の賞賛
返信

1,026件の閲覧回数
kaveeh
Contributor I

Hi James,

I got this file by our local support and not sure that have a right to share it. I can send you in private as you are NXP employee.

Best

0 件の賞賛
返信