The Camera Image is Split.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The Camera Image is Split.

ソリューションへジャンプ
3,248件の閲覧回数
donggyulee
Contributor I

Hi All,

I'm testing the camera of i.mx6 demo kit.

(The Board is SabreSD 6Q)

The camera image is not good.

The Camera image was split in two.

Please Check the attached file.

My System :

     Linux 3.0.101

     Camera Module : OV5640 Mipi

     Test command :  ./unit_tests/mxc_v4l2_overlay.out -iw 1920 -ih 1080 -ow 1920 -oh 1080 -di /dev/video1

Please advise.

Thank you

0 件の賞賛
返信
1 解決策
3,077件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi DongGyu

seems driver does not cover the 1080p 30fps option and although it’s theoretically possible

to achieve, it would require the coefficient  pair values to tweak the frame rate. These coefficient

tables are given by Omnivision. One can use drivers provided for other boards, like Sabre Lite board.

https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_3.10.17_1.0.0_ga/drivers/media/platf...

Alternatively one may look for other 3rd party efforts:

http://dl.linux-sunxi.org/SDK/A23-v1.0/unpacked/A23/lichee/linux-3.4/drivers/media/video/sunxi-vfe/d...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
3,078件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi DongGyu

seems driver does not cover the 1080p 30fps option and although it’s theoretically possible

to achieve, it would require the coefficient  pair values to tweak the frame rate. These coefficient

tables are given by Omnivision. One can use drivers provided for other boards, like Sabre Lite board.

https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_3.10.17_1.0.0_ga/drivers/media/platf...

Alternatively one may look for other 3rd party efforts:

http://dl.linux-sunxi.org/SDK/A23-v1.0/unpacked/A23/lichee/linux-3.4/drivers/media/video/sunxi-vfe/d...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

3,077件の閲覧回数
donggyulee
Contributor I

Hi igor

Thank you so much

You are a nice guy:smileyhappy:

0 件の賞賛
返信