UM805RE on the IMXUL 9x9 Ref design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UM805RE on the IMXUL 9x9 Ref design

2,139 Views
kaveeh
Contributor I

Hello,

What is the purpose of using U708 in the IMX6UL 9x9 Ref design?

I guess the external LDO U701 is also used to power-up the U708 from off mode. So, if we remove the U708 and populate the R758 then is it possible as well to remove the external LDO (U701).

Thanks,

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

886 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Kaveh,

I understand,  please create a  CASE,  using our  web page  http://nxp.com/support and click under the Hardware & Software, we can continue the discussion in private using that platform.

0 Kudos
Reply

885 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Kaveh,

Can you share the schematics that you are mention,  NXP only offers the i.MX6UL EVK board.  which does not use the 9x9 i.Mx6U device.

0 Kudos
Reply

886 Views
kaveeh
Contributor I

Hi James,

I got this file by our local support and not sure that have a right to share it. I can send you in private as you are NXP employee.

Best

0 Kudos
Reply