UI Performance in imx6 Quad for Android Kitkat

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UI Performance in imx6 Quad for Android Kitkat

1,798件の閲覧回数
teddy123
Contributor III

Hi Everyone,

As I tried to port Freescale package kk4.4.2_1.0.0-ga to my custom iMX6 Quad board, I encountered strange problems in the UI. After booting process gets completed, I was able to see red frames across the edges of the screen visible when I tried to access the UI. I did not have this problem with JellyBean. Is this issue related with GPU or Kikat OS?

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

1,578件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Ted,

Have you tried this with KK4.4.3 ?, this new release fixes GPU issues.


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,578件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello,

Are you able to post a photo of the red frames?, I have KK4.4.2.1 on the Sabre Quad and Dual Lite but I'm unable to see anything like that.

0 件の賞賛
返信