UART3, UART4, UART5 on imx6ull

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART3, UART4, UART5 on imx6ull

7,190 Views
stevenyu
Contributor III

Hi All,

We know the i.mx6ull has UART1 and UART2 enabled by default. 

In our board, we would like to use UART4, UART5, and then we have modify the device tree as below.

The result is TX from our board to PC console is OK. But RX from PC console to our board is no action (even no interrupts) Which thing we miss?

pinctrl_uart4: uart4grp {
fsl,pins = <
MX6UL_PAD_UART4_TX_DATA__UART4_DCE_TX 0x1b0b1
MX6UL_PAD_UART4_RX_DATA__UART4_DCE_RX 0x1b0b1
>;
};

pinctrl_uart5: uart5grp {
fsl,pins = <
MX6UL_PAD_UART5_TX_DATA__UART5_DCE_TX 0x1b0b1
MX6UL_PAD_UART5_RX_DATA__UART5_DCE_RX 0x1b0b1
>;
};

environment:

our board===UART4/UART5===usb2rs232----PC

echo "hello" > /dev/ttymxc4 is ok

but cat /dev/ttymxc4 does not receive message from PC teraterm console.

Regards,

Stephen 

Labels (1)
6 Replies

5,620 Views
joanxie
NXP TechSupport
NXP TechSupport

first try to confirm IOMUX configuration, is there conflict, then pls refer to the link as below

https://community.nxp.com/message/663015 

5,620 Views
zhichaohuang
Contributor II

I met the same problem.I use MCIMX6Y1CVM05AA on my board and uart5 can‘t receive data.But the uart5 is running correctly on MCIMX6Y2CVM05AA by using the same kernel and dts.

Is there any difference between the two cpus I missed?

0 Kudos
Reply

5,620 Views
zhichaohuang
Contributor II

I think I find the reason.In the imx6ul-pinfun.c define the pin of uart5:

#define MX6UL_PAD_UART5_RX_DATA__UART5_DCE_RX 0x00C0 0x034C 0x0644 0x0 0x5

But the input_val is for imx6ul as follow:

pastedImage_1.png

imx6ull's input_val is changed:

pastedImage_2.png

So I think the right value as below:

#define MX6ULL_PAD_UART5_RX_DATA__UART5_DCE_RX 0x00C0 0x034C 0x0644 0x0 0x7

5,620 Views
iohertz
Contributor II

Hi,

Have you tested your doubt. Is it working now?

0 Kudos
Reply

5,620 Views
zhichaohuang
Contributor II

yeah,I have tested.It's working on my board.:smileyhappy:

0 Kudos
Reply

5,620 Views
iohertz
Contributor II

Great. Can you help me with my problem?

I am facing the issue: https://community.nxp.com/thread/482578?sr=inbox 

0 Kudos
Reply