UART jitter spec at max speed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UART jitter spec at max speed

2,286 次查看
jakebailey
Contributor I

What is the tolerable jitter for imx6 UART at max speed of 4mbps?

The reference manual makes claims that there are new improvements to voting mechanism triggering that improve performance. Is this already accounted for in datasheet spec? From what I understand datasheet is claiming 6% jitter per bit with max 18% per 9bit word.

Our application requires 4mbps at up to 300m so I am trying to decide if RS485 drivers need equalization to reduce jitter or not.

Thanks.

标签 (2)
标记 (4)
0 项奖励
回复
1 回复

2,209 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 As stated, in the following, for example, considerations, the main question really

is how different the transmit and receive UART clocks can be. The clock mismatch

error about +/-2% is acceptable.

 

“Determining Clock Accuracy Requirements for UART Communications”

 

https://pdfserv.maximintegrated.com/en/an/AN2141.pdf

 

The voting scheme allows to improve noise immunity of data samples,

but in general clock accuracy considerations are the same, assuming

data are sampled at the center of bit period.

 


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复