UART functionality without RTS & CTS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART functionality without RTS & CTS

1,459 Views
Pavithra31R
Contributor I

We have a custom board design with i.MX 8M Nano processor. In this we are using all the 3/4 UART instances. 

UART3_RXD - E18
UART3_TXD - D18

We have not connected RTS & CTS as we don't require hardware flow control.

Is it possible to connect the UART without RTS and CTS?

Labels (1)
0 Kudos
Reply
1 Reply

1,455 Views
KalaimaniArumugamdev
Contributor III

Hi,

  Yes is possible, For custom design board you may disable the hardware flow control operations through software configurations.But in the

0 Kudos
Reply