U-boot configuration in Yocto Project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

U-boot configuration in Yocto Project

跳至解决方案
13,275 次查看
kanimozhi_t
Contributor V

Hi all,

    I’m building Yocto project from https://source.codeaurora.org/external/imx/imx-manifest/tree/imx-4.19.35-1.1.0.xml?h=imx-linux-warri... with mender for iMX 6UL EVK.

    Here u-boot consists of two parts (SPL & u-boot.img) rather than the single file u-boot-dtb.imx. It produces headache while integrating mender into the build or while signing the u-boot.

NOTE: generated images are listed in the attached picture

    I would like to know how & where to change the Yocto project build in order to produce the single .imx file. Any help would be much appreciated & thanks in advance.

    

标签 (3)
1 解答
13,088 次查看
kanimozhi_t
Contributor V

Thanks gusarambula‌,

 We managed to resolve it by changing the wks file used to build the .wic.gz image. Now our MACHINE.conf(conf/machine/imx6ulevk.conf) looks like,

UBOOT_SUFFIX = "imx"
# SPL_BINARY = "SPL"
WKS_FILE = "imx-uboot-bootpart.wks.in"

So, it now uses the single, produced .imx image. Sorry about not mentioning it earlier!

在原帖中查看解决方案

0 项奖励
回复
4 回复数
13,089 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kanimozhi Thangappan,

I do not have experience with Mender so I do not know how it may affect Yocto’s behavior, if it does.

As for the .imx bootloader file, it is generated by the imx-mkimage package, specifically the imx-boot recipe which is called bu the u-boot-imx recipe. Are you using u-boot-imx to generate the bootloader? This should be the preferred u-boot for the imx6ulevk MACHINE but I checked the imx6ulevk.conf file and it’s not specified so maybe just adding it may do the trick.

Ty opening the imx6ulevk configuration file:

imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/conf/machine/imx6ulevk.conf

And adding:

PREFERRED_PROVIDER_u-boot = "u-boot-imx"

And then bake the bootloader or image again.

I hope this helps!

Regards,

13,090 次查看
kanimozhi_t
Contributor V

Hey gusarambula‌,

    Thanks for your insights! I successfully changed the u-boot provider and able to build u-boot but when I attempted to build core-image-base image I encountered the below error.

test_yocto/test_build/tmp/work/imx6ulevk-fslc-linux-gnueabi/core-image-base/1.0-r0/temp/log.do_image_wic.596

ERROR: Function failed: do_image_wic (log file is located at /home/ux/test_yocto/test_build/tmp/work/imx6ulevk-fslc-linux-gnueabi/core-image-base/1.0-r0/temp/log.do_image_wic.596)
ERROR: Task (/home/ux/test_yocto/sources/poky/meta/recipes-core/images/core-image-base.bb:do_image_wic) failed with exit code '1'

    The reason is that do_wic_image expects imx6ulevk/SPL and there's no such file. Can you help me to resolve this error, so that the base image will use the produced .imx file to boot??

NOTE: The detailed log is attached here: imx6/do_image_wic.log at master · danie007/imx6 · GitHub 

0 项奖励
回复
13,090 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kanimozhi Thangappan,

I found another similar case on the communities for other kernel but the same MACHINE so I’m suspecting there may be other omissions on the machine configuration. I’ll try to reproduce and escalate this issue and I ‘will let you know as soon as I have more information.

Regards,

13,089 次查看
kanimozhi_t
Contributor V

Thanks gusarambula‌,

 We managed to resolve it by changing the wks file used to build the .wic.gz image. Now our MACHINE.conf(conf/machine/imx6ulevk.conf) looks like,

UBOOT_SUFFIX = "imx"
# SPL_BINARY = "SPL"
WKS_FILE = "imx-uboot-bootpart.wks.in"

So, it now uses the single, produced .imx image. Sorry about not mentioning it earlier!

0 项奖励
回复