U-Boot on I.Mx35

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-Boot on I.Mx35

1,812件の閲覧回数
m_f_vankessel
Contributor I

I'm trying to port U-Boot for an custom I.Mx35 board with only NAND-Flash, the board comes with an RedBoot bootloader.

Is there someone who has any experience with booting from NAND flash?

I have read some I.Mx configurations and I could only find one device booting directly from NAND (Karo - tx25, I.Mx25).

But I'm not sure if this will also work for the I.Mx35?!?

Max

タグ(5)
0 件の賞賛
返信
1 返信

1,573件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please refer to app note AN4172 (U-Boot® for i.MX35 Based Designs)

http://cache.freescale.com/files/dsp/doc/app_note/AN4172.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信