U-Boot PWM Test For Brightness

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-Boot PWM Test For Brightness

3,131件の閲覧回数
anshulkhare
Contributor III

Hi,

I have an iMX6UL board,
i am doing U-Boot PWM Test for Changing the brightness on LCD Display,
is there any command to perform the test in U-Boot .

Thank you :smileyhappy:

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,470件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Anshul

usually pwm is used in uboot for lcd brightness, seems

one can add special pwm commands using pwm driver in

drivers/pwm/pwm-imx.c. Pwm examples can be found in Github SDK
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,470件の閲覧回数
anshulkhare
Contributor III

Hi igor,

Thanks for Your Reply,

i am not getting which special command i need to enable in driver,

can u please help me on this.

Best regards
Anshul

0 件の賞賛
返信