Tuner si4763 RDS function in i.mx6 SABRE AI board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Tuner si4763 RDS function in i.mx6 SABRE AI board

2,489 次查看
AlbertH
Contributor II


Hello,

Does anyone have success on making the Tuner board Si4763 RDS function working on i.mx6 SABRE AI board?

The rest of functions are working fine. But I have problem on RDS function. it seems the interrupt is not trigger.

I appreciate any help on this.

Thanks in advance!

Albert

0 项奖励
回复
4 回复数

2,250 次查看
AlbertH
Contributor II

Thanks!

In the BSP 3.14.52 source code "radio-si476x.c", it has some RDS flag. I am not sure if that is something related RDS function.

Albert

0 项奖励
回复

2,250 次查看
AlbertH
Contributor II

I am using BSP 3.14.52. From the release notes of this version, it supported si4763. But the RDS is not working. And the RDS is even not included in the unit_test code.

The RDS has to trig the interrupt flag in status register, we monitor this flag and it has never been set. I.mx6 sabre AI board has interface to si4763 daughter board. If any IO used for interrupt, I think it should be in the interface.

0 项奖励
回复

2,250 次查看
jimmychan
NXP TechSupport
NXP TechSupport

The SI4763 on the SabreAI board is used for AM/FM tuner only. RDS is not implemented.

0 项奖励
回复

2,250 次查看
jimmychan
NXP TechSupport
NXP TechSupport

which BSP are you using? is the si4763 driver running well?

what you  mean the interrupt is not trigger? are you connecting the GPIO pin for interrupt?

0 项奖励
回复