Trying to build the yocto image with scarthgap 6.6.52 support for our custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trying to build the yocto image with scarthgap 6.6.52 support for our custom board

1,341 Views
arka
Contributor III

Hi ,

While trying to build the yocto image for imx8mm with scarthgap 6.6.52 support for our custom board , we have faced below error, how to solve?

arka_0-1739857596800.png

 

0 Kudos
Reply
3 Replies

1,316 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi

From the error message, "" No sandbox user '_apt' on the system, can not drop privileges",

I googled this and got lots of hits. You can refer to below suggestions.

Engelszüngeln: Fixing "No sandbox user" the Right Way

apt - No sandbox user '_apt' on the system, can not drop privileges - Ask Ubuntu

 

Regards

Daniel

0 Kudos
Reply

1,299 Views
arka
Contributor III

Hi ,

followed the above link steps , still i could not able to solve the error 

error:-

dpkg: warning: overriding problem because --force enabled:
dpkg: warning: package architecture (arm64) does not match system (amd64)

E: Sub-process dpkg returned an error code (1)


0 Kudos
Reply

1,275 Views
joanxie
NXP TechSupport
NXP TechSupport

how you build the 6.6.52 for imx8mm, which images and backed do you use? share the  build steps, let me reproduce this

0 Kudos
Reply