Trying to apply patch to Android running into error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Trying to apply patch to Android running into error

2,049 次查看
jsherman10
Contributor I

I'm currently trying to patch the Android Lollipop 5.0 code and I run into the following error:

The command I type to patch the code is:

c_patch ~/Downloads/android_L5.0.0_1.0.0-ga_core_source/code/l5.0.0_1.0.0-ga imx_l5.0.0_1.0.0-ga

Error:

Error! Base version commit fae26a039f79d780ddedcad07f164d9e6c05fc87 doesn't exist in git /home/jsherman/myandroid/prebuilts/clang/linux-x86/host/3.4.

I have read the instructions very carefully and cant seem to figure out the issue.

标签 (2)
标记 (2)
0 项奖励
回复
2 回复数

1,913 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jonathan Sherman,

It seems that there is a problem with the commit. Are you sure that the downloaded source code it’s the correct manifest? You may want to try to download the source code again. There are two Android 5 BSPs so there is a bit of room for mistakes.

I will try to reproduce the error. In the meantime another option is to switch to the L5.1.1_2.0.0 BSP.

Regards,

0 项奖励
回复

1,913 次查看
jsherman10
Contributor I

Thank you for your reply,

I actually need Android 5.0.0 specifically so it will run with this other open source software.  I will look at the manifest

0 项奖励
回复