Treck TCP/IP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Treck TCP/IP

2,453 Views
story
Contributor II

Hi,

        Recently, there has been a vulnerability issue in the Treck TCP/IP protocol library. Will the NXP i.MX8MM I use, the officially improved demo image and the cross-compilation chain tool have any impact? Is the Treck TCP/IP protocol library used?


https://www.jsof-tech.com/ripple20/

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

2,176 Views
amsec
Contributor I

Hi.

we have same doubt about Tcp/ip library.
"Does MQX TCP/IP stack have this vulnerability"
we are using K60 micro controller for network connectivity
please confirm on this.

Regards 

Saikiran.M

0 Kudos
Reply

2,176 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The TCP/IP library is used but it´s not from trek.But It can be implemented. Implements routing operations for TCP/UDP
connections:
− IPv4 with and without NAT
− IPv6
− VLAN tag insertion and removal

Regards

0 Kudos
Reply