Transferring data over EIM to iMX6 using DMA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Transferring data over EIM to iMX6 using DMA

1,756件の閲覧回数
sfoley
Contributor I

Hello,

I want to use SDMA to transfer data over EIM from a FIFO on a FPGA to the IMX6. I found this post https://community.nxp.com/t5/i-MX-Processors/working-SDMA-with-EIM-on-iMX6/m-p/276541 and was hoping I could get the example code mentioned by Weidong. If that example code is not available I would like to be pointed in the right direct for where I could read more documentation about SDMA with EIM.

 

Thanks,

Sean Foley

0 件の賞賛
返信
2 返答(返信)

1,692件の閲覧回数
ceggers1
Contributor IV

Hi Sean,

I looks like you want to transfer data from a fixed address (FPGA FIFO) to a continuous range of memory. Do you know the amount of data in advance, or do you have additional handshake signals for this (like FIFO empty)? Do you want the transfer to start "by hand" or should it start automatically as soon as data is available?

Most of the existing SDMA scripts like "ap_2_mcu" or "mcu_2_app" expect that there is a "DMA request" line from the peripheral to be monitored.

regards

Christian

0 件の賞賛
返信

1,727件の閲覧回数
art
NXP Employee
NXP Employee

Hello,

You can ask Weidong directly for the code he provided.

For general information, please refer to the "SDMA API" section of the i.MX Linux Reference Maual document for the Linux BSP you use.

Best Regards,
Artur

0 件の賞賛
返信