Toolchain for i.mx28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Toolchain for i.mx28

1,675 Views
tomhanks
Contributor I

I am trying to get a build going for i.mx28.  I've downreved Ubuntu to 10.10 which allows me to install LTIB, which seems to be required, but I can't get a g++ install for the old version of Ubuntu.  If I use a more recent version of Ubuntu, I can't get LTIB installed.

What's the current toolchain setup I should be using for a linux application for i.mx28?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,434 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tom

for new ubuntu one can look at suggestions provided on

imx6q build LTIB problems 

or use some third party yocto releases, like:

http://www.digi.com/support/productdetail?pid=5587&type=documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply