To select i.MX6 DI counter for active window HCOUNT and VCOUNT.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

To select i.MX6 DI counter for active window HCOUNT and VCOUNT.

跳至解决方案
835 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 IPU DI counter.

I consider what counter should I use for AW_HCOUNT and AW_VOUNT set by DIx_AW_xCOUNT_SEL field in IPU_DIx_AWx register.

Is there any restriction for couter selecting?

(e.g. same counter should be used for AW_HCOUNT and AW_VCOUNT)

Best Regards,

Satoshi Shimodaq

标记 (1)
0 项奖励
回复
1 解答
691 次查看
YixingKong
Senior Contributor IV

Satoshi

Here are response from our internal engineer. Please see if it helps you. You may reply with an update if you have any further inquery.
-----------------------------------------------------------------

We don't actually use IPU_DIx_AWx currently. What's the use case for it? From RM, I think if the counter, for, e.q, AW_HCOUNT not greater than HSYNC, should be ok.

------------------------------------------------------------------

Thanks,

Yixing

在原帖中查看解决方案

0 项奖励
回复
1 回复
692 次查看
YixingKong
Senior Contributor IV

Satoshi

Here are response from our internal engineer. Please see if it helps you. You may reply with an update if you have any further inquery.
-----------------------------------------------------------------

We don't actually use IPU_DIx_AWx currently. What's the use case for it? From RM, I think if the counter, for, e.q, AW_HCOUNT not greater than HSYNC, should be ok.

------------------------------------------------------------------

Thanks,

Yixing

0 项奖励
回复