To select i.MX6 DI counter for active window HCOUNT and VCOUNT.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

To select i.MX6 DI counter for active window HCOUNT and VCOUNT.

Jump to solution
739 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 IPU DI counter.

I consider what counter should I use for AW_HCOUNT and AW_VOUNT set by DIx_AW_xCOUNT_SEL field in IPU_DIx_AWx register.

Is there any restriction for couter selecting?

(e.g. same counter should be used for AW_HCOUNT and AW_VCOUNT)

Best Regards,

Satoshi Shimodaq

Tags (1)
0 Kudos
Reply
1 Solution
595 Views
YixingKong
Senior Contributor IV

Satoshi

Here are response from our internal engineer. Please see if it helps you. You may reply with an update if you have any further inquery.
-----------------------------------------------------------------

We don't actually use IPU_DIx_AWx currently. What's the use case for it? From RM, I think if the counter, for, e.q, AW_HCOUNT not greater than HSYNC, should be ok.

------------------------------------------------------------------

Thanks,

Yixing

View solution in original post

0 Kudos
Reply
1 Reply
596 Views
YixingKong
Senior Contributor IV

Satoshi

Here are response from our internal engineer. Please see if it helps you. You may reply with an update if you have any further inquery.
-----------------------------------------------------------------

We don't actually use IPU_DIx_AWx currently. What's the use case for it? From RM, I think if the counter, for, e.q, AW_HCOUNT not greater than HSYNC, should be ok.

------------------------------------------------------------------

Thanks,

Yixing

0 Kudos
Reply