Time shift after resume

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Time shift after resume

1,153件の閲覧回数
mathew_k_t
Contributor II

Hi,

I'm using iMX6ULL Board. I have two instances of the same device, both are connected as IIO devices.

These two devices produce ADC ready interrupts. Normally, it follows a difference of 5ms between the devices.

But, each time when the devices wake up from suspend mode 5ms is increased by 100usec.

What's the reason for this timeshift?

How to avoid it or maintain 5ms difference?

ラベル(3)
0 件の賞賛
返信
0 返答(返信)