This is veera

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

This is veera

4,840件の閲覧回数
veeranjaneyulug
Contributor III

Hi every one,

Have a good day.

we need to gst-rtsp-server package .This package i added in yocto setup core-image-minimal.bb file .But not showing in unit_test folder.

can u please tell me any body how to generate gst-rtsp-server binary in yocto setup

0 件の賞賛
返信
6 返答(返信)

4,661件の閲覧回数
veeranjaneyulug
Contributor III

Good morning every body.

Have a nice day.

Then i ran bitbake fsl-image-machine-test also run .But ie showing error.Actually my doubt is imx6qsabresd target board which gstreamer version is support ?.

Actual gst-rtsp_0.10.8.bb file is located at

The path is

sources/meta-openembedded/meta-multimedia/recipes-multimedia/gstreamer/gst-rtsp/

in the above path gst-rtsp .bb file located

0 件の賞賛
返信

4,661件の閲覧回数
veeranjaneyulug
Contributor III

Thank you for your guidence.

By using yocto setup in core-image-minimal.bb file i gave below packages.

gst-meta-video, gst-fsl-plugin, gst-plugins-base-app, gst-plugins-base ,gst-plugins-good, gst-plugins-good-rtsp, gst-plugins-good-udp, gst-plugins-good-rtpmanager, gst-plugins-good-rtp, gst-plugins-good-video4linux2 ,packagegroup-fsl-gstreamer.

The above package list all gst plugins are working the issue came from gst-fsl-plugin package any body body help me.

The error logs attached below

User1@FSETBLR1LX045:~/epdc/yocto/fsl-release-bsp/build$ bitbake core-image-minimal

Loading cache: 100% |##########################################################################################################| ETA:  00:00:00

Loaded 2193 entries from dependency cache.

NOTE: Resolving any missing task queue dependencies

NOTE: multiple providers are available for jpeg (jpeg, libjpeg-turbo)

NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg

NOTE: preferred version 3.10.53-1.1.0 of imx-lib not available (for item imx-lib)

NOTE: versions of imx-lib available: 1:3.0.35-4.0.0 1:3.10.17-1.0.0

NOTE: preferred version 3.10.53-1.1.0 of imx-lib not available (for item imx-lib)

NOTE: versions of imx-lib available: 1:3.0.35-4.0.0 1:3.10.17-1.0.0

NOTE: preferred version 3.10.53-1.1.0 of imx-lib not available (for item imx-lib-dev)

NOTE: versions of imx-lib available: 1:3.0.35-4.0.0 1:3.10.17-1.0.0

Build Configuration:

BB_VERSION        = "1.22.0"

BUILD_SYS         = "x86_64-linux"

NATIVELSBSTRING   = "Ubuntu-12.04"

TARGET_SYS        = "arm-poky-linux-gnueabi"

MACHINE           = "imx6dlsabresd"

DISTRO            = "poky"

DISTRO_VERSION    = "1.6.2"

TUNE_FEATURES     = "armv7a vfp neon callconvention-hard cortexa9"

TARGET_FPU        = "vfp-neon"

meta             

meta-yocto        = "(nobranch):30b8d9378b8260e452552b806610dc9b6fe0b69f"

meta-oe           = "(nobranch):8065dd8456913457a0114ddb2b4bd4842847b2a3"

meta-fsl-arm      = "(nobranch):9bc540eec9a7e280af13371ea70650fcc47ea627"

meta-fsl-arm-extra = "(nobranch):e1085deb3d915d2a95a65cceadc77c6de0dadfb6"

meta-fsl-demos    = "(nobranch):f141c7d1158b8addbd6f1ed047a1b47c2ed85f8f"

meta-fsl-arm     

meta-fsl-demos    = "(nobranch):0c5367e963b5f7797ded59f835313466b896d7e9"

meta-browser      = "(nobranch):63963cc56c8d0291779693e62b66cb16e5c86883"

meta-gnome       

meta-networking  

meta-ruby         = "(nobranch):8065dd8456913457a0114ddb2b4bd4842847b2a3"

meta-qt5          = "(nobranch):c29c317e0f22202bfaa85329a580564bbc179089"

meta-fsl-qt5     

meta-fsl-bluez    = "(nobranch):0c5367e963b5f7797ded59f835313466b896d7e9"

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

ERROR: Function failed: imx-lib: LIC_FILES_CHKSUM points to an invalid file: /home/User1/epdc/yocto/fsl-release-bsp/build/tmp/work/imx6dlsabresd-poky-linux-gnueabi/imx-lib/1_3.10.17-1.0.0-r0/imx-lib-3.10.17-1.0.0/ipu/mxc_ipu_hl_lib.h

ERROR: Logfile of failure stored in: /home/User1/epdc/yocto/fsl-release-bsp/build/tmp/work/imx6dlsabresd-poky-linux-gnueabi/imx-lib/1_3.10.17-1.0.0-r0/temp/log.do_configure.18683

Log data follows:

| DEBUG: Executing python function sysroot_cleansstate

| DEBUG: Python function sysroot_cleansstate finished

| DEBUG: Executing shell function do_configure

| DEBUG: Shell function do_configure finished

| DEBUG: Executing python function do_qa_configure

| NOTE: Checking autotools environment for common misconfiguration

| DEBUG: Python function do_qa_configure finished

| ERROR: Function failed: imx-lib: LIC_FILES_CHKSUM points to an invalid file: /home/User1/epdc/yocto/fsl-release-bsp/build/tmp/work/imx6dlsabresd-poky-linux-gnueabi/imx-lib/1_3.10.17-1.0.0-r0/imx-lib-3.10.17-1.0.0/ipu/mxc_ipu_hl_lib.h

ERROR: Task 1224 (/home/User1/epdc/yocto/fsl-release-bsp/sources/meta-fsl-arm/recipes-bsp/imx-lib/imx-lib_3.10.17-1.0.0.bb, do_configure) failed with exit code '1'

NOTE: Tasks Summary: Attempted 1991 tasks of which 1987 didn't need to be rerun and 1 failed.

Waiting for 0 running tasks to finish:

Summary: 1 task failed:

  /home/User1/epdc/yocto/fsl-release-bsp/sources/meta-fsl-arm/recipes-bsp/imx-lib/imx-lib_3.10.17-1.0.0.bb, do_configure

Summary: There was 1 ERROR message shown, returning a non-zero exit code.

0 件の賞賛
返信

4,658件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi veeranjaneyulu

core-image-minimal is small image that only allows a device to boot.

Suggest to build sl-image-machine-test, pelase check attached Yocto Guide

sect.5.1 Choosing a Freescale Yocto project image

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,658件の閲覧回数
veeranjaneyulug
Contributor III

Hi ,

Thanks for your suggestion .

Actually i need gst-rtsp-server plugin .How to built gstreamer latest

plugins and source with yocto setup .

As per user guide i run below commands but not showing in work folder

that gstreamer latest package.

RTSP Streaming Server

The RTSP streaming server usage case is based on the open source

gst-rtsp-server package. It uses the Freescale aiurdemux

plugin to demultiplex the file to audio or video elementary streams and

to send them out through RTP. You can start the

RTSP streaming server on one board, and play it on another board with

the RTSP streaming playback commands.

The gst-rtsp-server package is not installed by default in the Yocto

Project release. You can follow these steps to build and

install it.

1. Enable the layer–meta-openembedded/meta-multimedia:

Adding the line BBLAYERS +=

"$/sources/meta-openembedded/meta-multimedia" to the

configuration file /build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gst-rtsp/0.10.8-r0/gst-rtsp-0.10.8/

examples/.libs/

5. Flash the image.

Copy test-uri into /usr/bin on board and assign the executing permission

to it.

I followed above the steps but not showing in that related directory .If

you have any idea plz give guidence.

Thanks & Regards

veera

0 件の賞賛
返信

4,658件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

3.10.17 BSP is very old please use last 3.14.28

SABRE Board Reference Design|Freescale

~igor

0 件の賞賛
返信

4,658件の閲覧回数
veeranjaneyulug
Contributor III

Hi igor,

Thanks for your guidence i solved my issue as per user guide .

I have another problem how to resize the video by using

bitbake imx-test

i run the above command it will give some imx6 related binaries

generated.

in that i used mxc_ipudevtest.c test application. i used but image was

not resize .

Image capturing purpose i used below command ie working .

mxc_v4l2_capture.out -iw 320 -ih 240 -ow 320 -oh 240 -m 1 -fr 15 -d

/home/video0 -i 1 -c 20 /home/320_240_15fps.yuv -


> image capture

But resizing purpose i used below command but not resize and

./mxc_ipudevtest.out -C configfile outfile

but not resize .

i used gstreamer plugin also.

gst-launch

gst-inspect

plz can u explore all this to me .

Thanks and regards

Veera

0 件の賞賛
返信