There is some lib missing when build Firefox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

There is some lib missing when build Firefox

1,794件の閲覧回数
wangvictor
Contributor III

Hi All:

I am using Firefox as my browser with x11.

I build firefox with this command `bitbake firefox`.

It all fine during the compiling.

But here is the problem when I execute firefox in my rootfs.

Here is the error that I got:

XPCOMGlueLoad error for file /usr/lib/firefox-38.4/libxul.so:

libvpx.so.2: Cannot open shared object file: No such file or directory

Couldn't load XPCOM.

When I check the library that yocto project built out and found no libvpx.so.2.

How to solve this question?

Thanks in Advanced.

ラベル(4)
タグ(3)
0 件の賞賛
返信
1 返信

1,555件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Wang

for firefox one can check boundary devices releases:

Morty Yocto Release i.MX6 Series - NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信