The iMx6 Chip Errata - Linux BSP solution status

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The iMx6 Chip Errata - Linux BSP solution status

4,984 Views
kenlin
Contributor II

Hi,

 

I would like to check the iMx6 errata solution phase-in status in kernel 4.8 and u-boot 2016.10 and tried to filter out the items that come with software solution before (the patches in previous iMx6 BSP releases e.g. imx_3.0.35_4.1.0, .. ) in the table below. 

I'm not sure how to check the software solutions to the errata items (marked in yellow) below. Need to get the feedback/comments from NXP team.

ERR005852, ERR003740,ERR005185,ERR005200,ERR009604,ERR006223,ERR009219,ERR005174,ERR004366,ERR009623,ERR005193,ERR005778,ERR005184,ERR009619,ERR009624,ERR007266,ERR009598,ERR008990,ERR004534,ERR006308,ERR004535,ERR007881,ERR004345,ERR004363

 

Errata number

Category

Description

In kernel 4.8 ?

In u-boot 2016.10 ?

ERR005852

Analog

Analog: Transition from Deep Sleep Mode to LDO Bypass Mode may cause the slow

 

 

ERR003718

ARM

ARM: 743622—Faulty logic in the Store Buffer may lead to data corruption

 

v

ERR003720

ARM/MP

ARM/MP: 751472—An interrupted ICIALLUIS operation may prevent the completion of a following broadcast operation

 

v

ERR003724

ARM

ARM: 754322—Possible faulty MMU translations following an ASID switch

v

 

ERR003740

ARM/PL310

ARM/PL310: 752271—Double linefill feature can cause data corruption [i.MX 6Dual/6Quad only]

 

 

ERR004325

ARM/MP

ARM/MP: 764369—Data or unified cache line maintenance operation by MVA may not succeed on an Inner Shareable memory region

v

 

ERR005185

ARM/MP

ARM/MP: 771225—Speculative cacheable reads to aborting memory region clear the internal exclusive monitor, may lead to livelock

 

 

ERR005199

ARM/MP

ARM/MP: 769419—No automatic Store Buffer drain, visibility of written data requires an explicit Cache Sync operation [i.MX 6Dual/6Quad Only]

v

 

ERR005200

ARM/MP

ARM/MP: 765569—Prefetcher can cross 4 KB boundary if offset is programmed with
value 23

 

 

ERR005383

ARM/MP

ARM/MP: 775420—A data cache maintenance operation that aborts, followed by an ISB and without any DSB in-between, might lead to deadlock

v

 

ERR007006

ARM/MP

ARM/MP:794072-- Short loop including a DMB instruction might cause a denial of
service

 

v

ERR009604

ARM (CA9)

ARM (CA9): 845369 — Under very rare timing circumstances, transition into streaming mode might create a data corruption

 

x

ERR009605

ARM (CA9)

ARM (CA9): 761320—Full cache line writes to the same memory region from at least two processors might deadlock the processor

 

v

ERR006223

CCM

CCM: Failure to resume from Wait/Stop mode with power gating

 

 

ERR007265

CCM

CCM: When improper low-power sequence is used, the SoC enters low power mode before the ARM core executes WFI

v

 

ERR009219

CCM

CCM: Asynchronous clock switching can cause unpredictable behavior [i.MX6 Dual/6Quad Only]

 

 

ERR009165

eCSPI

eCSPI: TXFIFO empty flag glitch can cause the current FIFO transfer to be sent twice

v

 

ERR006358

ENET

ENET: Write to Transmit Descriptor Active Register (ENET_TDAR) is ignored

v

 

ERR006687

ENET

ENET: Only the ENET wake-up interrupt request can wake the system from Wait

v

 

ERR004323

HDMI

HDMI: The DMA burst read transaction address region is limited to 8 KB

v

 

ERR005171

HDMI

HDMI: HDMI Tx audio may have noise due to audio DMA FIFO overflow

v

 

ERR005173

HDMI

HDMI: Clarification on HDMI programming procedure to avoid FIFO overflow

v

 

ERR005174

HDMI

HDMI: HDMI AHB Audio DMA stream misalignment on system initialization

 

 

ERR004366

HDMI

HDMI: 9000482480—ARM core read operation returns incorrect data for certain HDCP registers

 

 

ERR009623

IPU

IPU: IDMAC burst errors when crossing a 4k boundary using NI/PI 420/422 formats [i.MX 6DualPlus/6QuadPlus Only]

 

 

ERR005193

MIPI

MIPI: Corruption of short command packets with Word Count (WC) greater than 16’hFFEE, during video mode transmission by the MIPI Generic Interface

 

 

ERR005778

MMDC

MMDC: DDR Controller’s measure unit may return an incorrect value when operating below 100 MHz

 

 

ERR005184

PCIe

PCIe: Clock pointers can lose sync during clock rate changes

 

 

ERR008587

PCIe

PCIe: Random link down after warm reset [i.MX 6Dual/6Quad Only]

v

 

ERR009619

PRE

PRE: GPU3D, GPU2D and VPU cannot be power-gated if the PRE is in use [i.MX 6DualPlus/6QuadPlus Only]

 

 

ERR009624

PRE

PRE: ENABLE bit cannot be set in a special case, when the EN_REPEAT bit is set [i.MX 6DualPlus/6QuadPlus Only]

 

 

ERR007266

ROM

ROM: EIM NOR boot may fail if plug-in is used

 

 

ERR007966

SATA

SATA:SATA speed negotiation fails after suspend and resume —[i.MX 6Dual/6Quad Only]

 

 

ERR009598

SATA

SATA: PRD not flushed from PRD FIFO at command list underflow

 

 

ERR008990

SSI

SSI: Channel swap in single FIFO mode when an underrun or overrun occurs

 

 

ERR004534

USB

USB: Wrong HS disconnection may be generated after resume

 

 

ERR006308

USB

USB: Host non-doubleword –aligned buffer address can cause host to hang on OUT Retry

 

 

ERR004535

VPU

VPU: Wrong interrupt is generated sometimes when context switching to H.264
encoder, during multi-instance

 

 

ERR007881

USB

USB: Timeout error in Device mode

 

 

ERR004345

USB

USB: USB suspend and resume flow clarifications

 

 

ERR004363

VPU

VPU: Causes a macro-block of P-picture decoding error

 

 

ERR004346

WDOG

WDOG: WDOG SRS bit requires to be written twice

v

 

Labels (3)
Tags (1)
0 Kudos
Reply
1 Reply

2,857 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ken

kernel 4.8 and u-boot 2016.10 are not supported by nxp, nxp official bsps located on link

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

and errata status is described in Errata document as "Linux BSP Status" for each item i.MX6DQ Errata

http://cache.freescale.com/files/32bit/doc/errata/IMX6DQCE.pdf

Please check difference between NXP(FSL) official BSP and NXP(FSL) community BSP

https://community.freescale.com/message/402940#402940

For kernel 4.8 one can post on mainline kernel mail list.


================================================================
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply