The four phys connected to sja1105Q cannot be loaded normally and work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The four phys connected to sja1105Q cannot be loaded normally and work

871件の閲覧回数
jinhuachen
Contributor II

The fec2 of the imx8qm is connected to the sja1105Q. The sja1105 is connected to four channels of phy. When the fec2 network port is initialized, mdio scans all the phys on the bus. At this time, the sja1105Q has not been initialized, so the phy mode of the phys on the mdio bus cannot be determined. As a result, the phys connected to the mdio cannot probe. so the phy cannot work normally.

Software version imx-automotive-11.0.0_ 2.5.0

&fec2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_fec2>;
phy-mode = "rgmii-id";
fsl,magic-packet;
nvmem-cells = <&fec_mac1>;
nvmem-cell-names = "mac-address";
fsl,mii-exclusive;
status = "okay";

fixed-link {
speed = <1000>;
full-duplex;
};

mdio {
#address-cells = <1>;
#size-cells = <0>;

fec2_ethphy1: ethernet-phy@1 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <0x1>;
};

fec2_ethphy2: ethernet-phy@2 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <0x2>;
};

fec2_ethphy8: ethernet-phy@8 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <0x8>;
};

fec2_ethphy9: ethernet-phy@9 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <0x9>;
};

};
};

&lpspi1 {
#address-cells = <1>;
#size-cells = <0>;
fsl,spi-num-chipselects = <1>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lpspi1 &pinctrl_lpspi1_cs>;
cs-gpios = <&lsio_gpio3 24 GPIO_ACTIVE_LOW>;
status = "okay";

switch: sja1105@0 {
compatible = "nxp,sja1105q";
reg = <0x0>;
reset-gpios = <&lsio_gpio1 7 GPIO_ACTIVE_LOW>;
spi-max-frequency = <4000000>;
spi-cpha;
fsl,spi-cs-sck-delay = <1000>;
fsl,spi-sck-cs-delay = <1000>;
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
label = "swp0";
ethernet = <&fec2>;
phy-mode = "rgmii-id";
reg = <0>;
fixed-link {
speed = <1000>;
full-duplex;
};
};
port@1 {
label = "swp1";
phy-mode = "mii";
phy-handle = <&fec2_ethphy8>;
reg = <1>;
};
port@2 {
label = "swp2";
phy-mode = "mii";
phy-handle = <&fec2_ethphy9>;
reg = <2>;
};
port@3 {
label = "swp3";
phy-mode = "rgmii-id";
phy-handle = <&fec2_ethphy1>;
reg = <3>;
};
port@4 {
label = "swp4";
phy-mode = "rgmii-id";
phy-handle = <&fec2_ethphy2>;
reg = <4>;
};
};
};
};

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

801件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @jinhuachen,

Please try adding the below configuration option in UBoot to test with mdio commands:

CONFIG_PHYLIB
CONFIG_CMD_MII

 

And after that, please Try to get the outputs of the Previously mentioned commands to see if PHYs are correctly detected.

 

I hope it helps!

Thanks & Regards,
Dhruvit.

0 件の賞賛
返信

831件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @jinhuachen,

One can try debugging with the below u-boot commands:
 
# mdio list
# mii info
 
Please provide me with full boot logs for further debugging, and kindly make sure that PHY addresses are configured correctly on the hardware side.
 
 
Best regards,
Dhruvit.
0 件の賞賛
返信

822件の閲覧回数
jinhuachen
Contributor II

Uboot does not debug phy. It only debugs on the kernel. The appendix contains the schematic diagram and boot log. Please check it

0 件の賞賛
返信

866件の閲覧回数
jinhuachen
Contributor II
[ 2.262823] mdio_bus 5b050000.ethernet-1: MDIO device at address 1 is missing.
[ 2.270121] mdio_bus 5b050000.ethernet-1: MDIO device at address 2 is missing.
[ 2.277418] mdio_bus 5b050000.ethernet-1: MDIO device at address 8 is missing.
[ 2.284712] mdio_bus 5b050000.ethernet-1: MDIO device at address 9 is missing.
0 件の賞賛
返信