The entry of data link layer(OS:linux) ,when using command "ping www.baidu.com"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The entry of data link layer(OS:linux) ,when using command "ping www.baidu.com"

1,244 次查看
liuyonggang
Contributor III

Platform:Imx8qxp

Environment:Yocto

OS:linux

Question:

I want to know the entry of data link layer(OS:linux) ,when using command "ping www.baidu.com",because I want to add some log to check ping data package(ping command lose package sometimes).

Can somebody help me?

BRs

Johnny

0 项奖励
回复
1 回复

1,209 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Johnny,

The ping function is included as part of the networking utilities included on the Yocto BSPs from Open Embedded.

You can find more information for this package if you look at the fping recipe inside Yocto. Inside the recipe you can find the repository for this package’s source code.

I hope this helps!

Regards,

0 项奖励
回复