The entry of data link layer(OS:linux) ,when using command "ping www.baidu.com"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The entry of data link layer(OS:linux) ,when using command "ping www.baidu.com"

1,257 Views
liuyonggang
Contributor III

Platform:Imx8qxp

Environment:Yocto

OS:linux

Question:

I want to know the entry of data link layer(OS:linux) ,when using command "ping www.baidu.com",because I want to add some log to check ping data package(ping command lose package sometimes).

Can somebody help me?

BRs

Johnny

0 Kudos
Reply
1 Reply

1,222 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Johnny,

The ping function is included as part of the networking utilities included on the Yocto BSPs from Open Embedded.

You can find more information for this package if you look at the fping recipe inside Yocto. Inside the recipe you can find the repository for this package’s source code.

I hope this helps!

Regards,

0 Kudos
Reply