The correct sequence to load the iMX USB modules when built the USB drivers as module -blog archive

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The correct sequence to load the iMX USB modules when built the USB drivers as module -blog archive

1,249件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee

1. modprobe fsl_otg_arc

2. modprobe ehci_hcd

3. modprobe arcotg_udc

4. modprobe g_ether

 

It was tested on L2.6.35_11.09_ER_SOURCE BSP.

タグ(1)
0 件の賞賛
返信
0 返答(返信)