The USB not recognized

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The USB not recognized

3,063 Views
937556508
Contributor I

Hi,

We use the MIMX8MM5DVTLZAA chip to carry the circuit design. Now the USB1 interface used to download the image is not recognized. Can you help me?

We are designing with reference to the USB2 circuit of the 8MMINILPD4-EVK development board. The following figure has additional circuit diagrams alarge.pngUSB不识别.PNGnd unidentified signs. and the PIN of USB1_ID is NC.

0 Kudos
Reply
3 Replies

3,059 Views
937556508
Contributor I

I'm very sorry that my description looks a bit confusing, let me reorganize it.

 

We use the MIMX8MM5DVTLZAA chip to carry the circuit design. Now the USB1 interface used to download the image is not recognized. Can you help me?

We are designing with reference to the USB2 circuit of the 8MMINILPD4-EVK development board. The following figure has additional circuit diagrams and unidentified signs. and the PIN of USB1_ID is NC.

Best regards.

0 Kudos
Reply

3,048 Views
igorpadykov
NXP Employee
NXP Employee

Hi 937556508

 

one can recheck usb connections using checklist in

i.MX 8M Mini Hardware Developer’s Guide

try to test it for example in linux, booting from  sd or emmc. For preparing boot

image try sect.4.3.2 Copying the full SD card image i.MX Linux User’s Guide​

 

Best regards
igor

0 Kudos
Reply

3,035 Views
937556508
Contributor I

Hi igor

Thank you very much for your reply.

I checked my circuit and think it is ok.

My board only has emmc boot, and there is no emmc card slot, so I have no way to download the boot image to emmc in advance.

Do you have other ways to help me?

In addition, I use the USB-type-C interface, is it a type-c problem?

Looking forward to your help.

 

Best regards

0 Kudos
Reply