The SPI1 does not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The SPI1 does not work

1,872 Views
kevinpwchen
Contributor II

Hi Sir,

We need to control SPI device via SPI1. However, it does not work well (the CLK always keeps in low). Do you have any ideas about that?  I can see these SPI nodes by ls -al /sys/class/spidev/ command as below:

root@imx8qxpmek:~# ls -al /sys/class/spidev/

drwxr-xr-x    2 root     root             0 Oct  3 05:44 .

drwxr-xr-x   63 root     root             0 Oct  3 05:44 ..

lrwxrwxrwx    1 root     root             0 Oct  3 05:44 spidev32763.0 -> ../../devices/platform/5a030000.lpspi/spi_master/spi32763/spi32763.0/spidev/spidev32763.0

lrwxrwxrwx    1 root     root             0 Oct  3 05:44 spidev32764.0 -> ../../devices/platform/5a020000.lpspi/spi_master/spi32764/spi32764.0/spidev/spidev32764.0

lrwxrwxrwx    1 root     root             0 Oct  3 05:44 spidev32765.0 -> ../../devices/platform/5a010000.lpspi/spi_master/spi32765/spi32765.0/spidev/spidev32765.0

lrwxrwxrwx    1 root     root             0 Oct  3 05:44 spidev32766.0 -> ../../devices/platform/5a000000.lpspi/spi_master/spi32766/spi32766.0/spidev/spidev32766.0

root@imx8qxpmek:~#

 

Below is what I configured in dts and dtsi files.

.dts file:

pinctrl_lpspi1: lpspi1grp {
fsl,pins = <
SC_P_SAI0_TXFS_ADMA_SPI1_SCK 0xD600004c
SC_P_SAI0_TXD_ADMA_SPI1_SDO 0xD600004c
SC_P_SAI0_TXC_ADMA_SPI1_SDI 0xD600004c
// SC_P_SAI0_RXD_ADMA_SPI1_CS0 0xD600004c
>;
};


pinctrl_lpspi1_cs: lpspi1cs {
fsl,pins = <
SC_P_SAI0_RXD_LSIO_GPIO0_IO27 0xE0000021
>;
};

......

&lpspi1 {
#address-cells = <1>;
#size-cells = <0>;
fsl,spi-num-chipselects = <1>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lpspi1 &pinctrl_lpspi1_cs>;
cs-gpios = <&gpio0 27 GPIO_ACTIVE_LOW>;
status = "okay";

spidev@0 {
compatible = "rohm,dh2228fv";
status = "okay";
spi-max-frequency = <1000000>;
reg = <0>;
};

};

 

dtsi file:

lpspi1: lpspi@5a010000 {
compatible = "fsl,imx7ulp-spi";
reg = <0x0 0x5a010000 0x0 0x10000>;
interrupts = <GIC_SPI 217 IRQ_TYPE_LEVEL_HIGH>;
interrupt-parent = <&gic>;
clocks = <&clk IMX8QXP_SPI1_CLK>,
<&clk IMX8QXP_SPI1_IPG_CLK>;
clock-names = "per", "ipg";
assigned-clocks = <&clk IMX8QXP_SPI1_CLK>;
assigned-clock-rates = <20000000>;
power-domains = <&pd_dma_lpspi1>;
status = "disabled";
};

Best regards

Kevin

0 Kudos
Reply
1 Reply

1,480 Views
danwei_luo
NXP Employee
NXP Employee

Hi Kevin,

Previously there is a typo in CLK driver, please check following changes is added:

clk-imx8qxp.c

 

clks[IMX8QXP_SPI1_CLK] = imx_clk_gate_scu("spi1_clk", "spi1_div", SC_R_SPI_2, SC_PM_CLK_PER, (void __iomem *)(LPSPI_1_LPCG), 0, 0);

 

change to :

 

clks[IMX8QXP_SPI1_CLK] = imx_clk_gate_scu("spi1_clk", "spi1_div", SC_R_SPI_1, SC_PM_CLK_PER, (void __iomem *)(LPSPI_1_LPCG), 0, 0);

Best regards,

Danwei

0 Kudos
Reply