The Git for Freescale BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The Git for Freescale BSP

5,475件の閲覧回数
JoaoPaulo
Contributor I

Hi


I'm trying to clone the IMX-BSP using the link http://opensource.freescale.com/pub/scm/imx/linux-2.6-imx.git.
When I run "git clone" git find the link but not download files.
Does anyone know a procedure to download these files?


Thanks


João Paulo

ラベル(1)
6 返答(返信)

1,767件の閲覧回数
JoaoPaulo
Contributor I

Hi.... 


It workedSuccessfully downloaded the repository using the link git://git.freescale.com/imx/linux-2.6-imx.git


Thanks for all.


João Paulo

1,767件の閲覧回数
santoshkadam
Contributor I

hi ,

What are the sizes of these repositories ? For me - it's more than 710 MB and is still continuing..BTW -- the link git://git.freescale.com/imx/linux-2.6-imx.git  is not working for me. I had to try the link - http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git

It is going on for a while now... Any help on sizes of these repositories?

Thx

San

0 件の賞賛
返信

1,767件の閲覧回数
DmitriyKiselev
Contributor I

Actually I put it to run on my server under screen, so, I really do not know how much time it took (it is VERY slow) but finally I got it cloned.

0 件の賞賛
返信

1,767件の閲覧回数
PeterTeoh
Contributor I

Oh, yes, me too:

Initialized empty Git repository in /home/tthtlc/imx53/linux-2.6-imx/.git/
error: Unable to get pack index http://opensource.freescale.com/pub/scm/imx/linux-2.6-imx.git/objects/pack/pack-2f40c4cf0a2e436bfcf6...

error: Unable to get pack index http://opensource.freescale.com/pub/scm/imx/linux-2.6-imx.git/objects/pack/pack-14df3fc7b39114254e28...

error: Unable to get pack index http://opensource.freescale.com/pub/scm/imx/linux-2.6-imx.git/objects/pack/pack-d7b21c0dfeace6fb5d6e...

error: Unable to get pack index http://opensource.freescale.com/pub/scm/imx/linux-2.6-imx.git/objects/pack/pack-c0cf604cbd4222cb647b...

error: Unable to find bc676214b92db468c7b72dc495312809dbfc37bf under http://opensource.freescale.com/pub/scm/imx/linux-2.6-imx.git
Cannot obtain needed object bc676214b92db468c7b72dc495312809dbfc37bf
while processing commit c57e4f2be8c66cd40d8c8a40a907a5a051f973df.
error: Fetch failed.

I think there is something wrong at the server side.

0 件の賞賛
返信

1,767件の閲覧回数
CurtisWald
NXP Employee
NXP Employee

Hi,
You might try http://git.freescale.com

And the Linux GIT tree would be: http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git which at the bottom has the clone URL for git.

-Curtis

0 件の賞賛
返信

1,767件の閲覧回数
TugrulGuclu
Contributor I

Hi

Have you made sure that access to port 9418 is allowed ?

I had a problem with git because of company firewall before.

0 件の賞賛
返信