The Differences between CMOS and Schmitt Trigger in HYS Bit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The Differences between CMOS and Schmitt Trigger in HYS Bit

4,869 次查看
tony_l_cai
Contributor III

Hi, all

     in MX6SL/DL, I dont know the option about the input type between CMOS trigger and schmitt trigger in HYS bit(1 bit hysteresis control),could you tell me in detail how to select these bits in different conditions?

3Q~

标签 (2)
0 项奖励
回复
1 回复

4,493 次查看
igorpadykov
NXP Employee
NXP Employee

Hi tony

when HYS=0, DISABLED — CMOS input, then

VIH,VIL are defined in Table 23. GPIO DC Parameters IMX6SDLCEC

when HYS=1, ENABLED — Schmitt trigger input, then

Input Hysteresis is turned on at input curcuit (see Table 23)

Hysteresis - Wikipedia, the free encyclopedia

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复