TJA1100 Rx and Tx Failure Count

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1100 Rx and Tx Failure Count

1,637 Views
yuvaraj_ayyasam
Contributor I

Hi Community,

I have a question about the TJA1100. We are using TJA1100 PHY for our automotive applications with the i.MX6 Dual Plus combination. We have requirement to fetch PHY Rx and Tx failure count. We gone through the TJA1100 PHY datasheet, I find

1) Link fail counter register (Register 26)

      * LOC_RCVR_CNT[15:8] &

      * REM_RCVR_CNT[7:0])

             (or)

2) Communication status register (Register 23)

      * RECEIVE_ERR[4] &

      * TRANSMIT_ERR [3]

Which register we need to prefer to counting receiver error count and transmit error count.

I have the following doubts,

1) If register 26 is correct, then shall we assume like below

     Local receiver count(LOC_RCVR_CNT) = Tx failure

     Remote receiver count(REM_RCVR_CNT) = Rx Failure

        (or)

2) If register 23 is correct, then shall we assume like below

     RECEIVE_ERR = We need to increase the count as Rx failure, as soon as this bit is enabled.

     TRANSMIT_ERR = We need to increase the count as Rx failure, as soon as this bit is enabled.

Could someone please clarify my doubt.

 

Thanks,

UVee

0 Kudos
Reply
1 Reply

1,539 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Yuvaraj,

I would recommend you to create a standard  support request as this needs to reviewed by product specialists or local FAEs. 

 

Thank you for your understanding!

 

Best regards,

Tomas

0 Kudos
Reply