TJA1043 wakeup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1043 wakeup

2,276件の閲覧回数
ysu
Contributor I

TJA1043: Did it can be wake up by wakeup pin, but not the CAN frame? that means, we need the IC wakeup only by wakeup pin, and the CAN frame not available.thanks

0 件の賞賛
返信
2 返答(返信)

1,987件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi shuang

The CAN controller can able to read back its own sent messages even though the bus line is open.

Hence, there won't be a chance of transmit error count, only the receive error count will get increased due to no acknowledgement. So, "Bus Off" will not happen when CANH or CANL is disconnected from the network.

0 件の賞賛
返信

1,987件の閲覧回数
ysu
Contributor I

Sorry, I didn't understand. What I want to know is, if only the wakeup pin available, but the CAN message wake up not available for the TJA1043? thanks

0 件の賞賛
返信