TIMER AND SPI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TIMER AND SPI

1,723 次查看
2548903578
Contributor III

use SPI and timer respectively, which are good, but an error occurs when the timer uses spi to read the chip data. Why is this? I am using the imx6sx board. The kernel version is linux imx6sxsabresd 5.4.24-2.1.0+gbabac008e5cf #1 SMP PREEMPT Sun Jan 31 06:20:10 UTC 2021 armv7l GNU/Linux. The error message is as follows:

 BUG: scheduling while atomic: swapper/0/0/0x00000102
[  698.793258] Modules linked in: di(O) [last unloaded: di]
[  698.798621] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G           O      5.4.24-2.1.0+gbabac008e5cf #1
[  698.807678] Hardware name: Freescale i.MX6 SoloX (Device Tree)
[  698.813566] [<801107b8>] (unwind_backtrace) from [<8010b684>] (show_stack+0x10/0x14)
[  698.821344] [<8010b684>] (show_stack) from [<80bd6aec>] (dump_stack+0x90/0xa4)
[  698.828595] [<80bd6aec>] (dump_stack) from [<80154338>] (__schedule_bug+0x70/0x84)
[  698.836195] [<80154338>] (__schedule_bug) from [<80bee434>] (__schedule+0x3b4/0x4cc)
[  698.843957] [<80bee434>] (__schedule) from [<80bee5ac>] (schedule+0x60/0x104)
[  698.851118] [<80bee5ac>] (schedule) from [<80bf23f8>] (schedule_timeout+0x168/0x288)
[  698.858886] [<80bf23f8>] (schedule_timeout) from [<80bef614>] (wait_for_completion_timeout+0xb0/0x124)
[  698.868228] [<80bef614>] (wait_for_completion_timeout) from [<806f5e54>] (spi_imx_transfer+0x2d0/0x464)
[  698.877648] [<806f5e54>] (spi_imx_transfer) from [<806f039c>] (spi_bitbang_transfer_one+0x50/0xa0)
[  698.886645] [<806f039c>] (spi_bitbang_transfer_one) from [<806ed448>] (spi_transfer_one_message+0x198/0x468)
[  698.896501] [<806ed448>] (spi_transfer_one_message) from [<806eda10>] (__spi_pump_messages+0x2f8/0x53c)
[  698.905915] [<806eda10>] (__spi_pump_messages) from [<806ede08>] (__spi_sync+0x1a8/0x1b0)
[  698.914109] [<806ede08>] (__spi_sync) from [<806ede34>] (spi_sync+0x24/0x3c)
[  698.921197] [<806ede34>] (spi_sync) from [<7f0003a0>] (mcp23s17_read_regs.constprop.0+0xe8/0x134 [di])
[  698.930547] [<7f0003a0>] (mcp23s17_read_regs.constprop.0 [di]) from [<7f000424>] (timer_function+0x38/0x74 [di])
[  698.940759] [<7f000424>] (timer_function [di]) from [<80190be4>] (call_timer_fn.constprop.0+0x24/0x98)
[  698.950089] [<80190be4>] (call_timer_fn.constprop.0) from [<8019127c>] (run_timer_softirq+0x3e0/0x3f8)
[  698.959420] [<8019127c>] (run_timer_softirq) from [<801022ac>] (__do_softirq+0x104/0x278)
[  698.967634] [<801022ac>] (__do_softirq) from [<80135690>] (irq_exit+0xb0/0xd8)
[  698.974895] [<80135690>] (irq_exit) from [<80178328>] (__handle_domain_irq+0x60/0xb0)
[  698.982763] [<80178328>] (__handle_domain_irq) from [<8049e4d8>] (gic_handle_irq+0x4c/0x90)
[  698.991142] [<8049e4d8>] (gic_handle_irq) from [<80101a8c>] (__irq_svc+0x6c/0xa8)
[  698.998635] Exception stack(0x81201f20 to 0x81201f68)
[  699.003712] 1f20: 00000000 000245e4 9f9b69f4 801199c0 81200000 00000000 81204f28 81204f64
[  699.011908] 1f40: 81185670 00000000 81201f78 00000000 00000000 81201f70 80108904 80108908
[  699.020095] 1f60: 600f0013 ffffffff
[  699.023614] [<80101a8c>] (__irq_svc) from [<80108908>] (arch_cpu_idle+0x38/0x3c)
[  699.031043] [<80108908>] (arch_cpu_idle) from [<8015abac>] (do_idle+0x22c/0x29c)
[  699.038464] [<8015abac>] (do_idle) from [<8015af10>] (cpu_startup_entry+0x18/0x1c)
[  699.046063] [<8015af10>] (cpu_startup_entry) from [<81100da8>] (start_kernel+0x458/0x484)QQ截图20210304170520.pngQQ截图20210304170520.pngQQ截图20210304170539.pngQQ截图20210304170539.pngQQ截图20210304170655.pngQQ截图20210304170655.png

0 项奖励
回复
2 回复数

1,709 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Is it a driver program? or your program running in user space? have you try to use ioctl like spidev?

0 项奖励
回复

1,701 次查看
2548903578
Contributor III

I just added the work queue

0 项奖励
回复