TAMPER i.MXULL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TAMPER i.MXULL

1,153件の閲覧回数
ban45
Contributor III

Hi

What  is iMX ULL TAMPER0~9 pins used for?

If you don't use it, is floart all right?

regard

0 件の賞賛
返信
1 返信

1,146件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ban45

 

information about tamper usage can be found in

Security Reference Manual for the i.MX 6ULL Applications Processor

or  https://www.iwavesystems.com/blog/imx6-module-imx6ul3-sodimm-som/

When not used recommended to to connect external 1M Ohm pull-up or pull-down resistors

to the pad to avoid the undesired leakage as described on Foot note 2 Table 91  p.121

i.MX 6ULL Applications Processors for Consumer Products

 

Best regards
igor

0 件の賞賛
返信