Synchronizing between drivers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Synchronizing between drivers

1,269件の閲覧回数
mathew_k_t
Contributor II

Hi,

I'm using imx6ull based board.

I have a connected same ADC device in ecspi3 and ecspi4. So that it uses the same device driver.

Each device generated ADC ready interrupts at every 10 msec.

I would like to implement a 5msec delay between the devices. i.e. if I'm getting interrupt from device1 first means after 5msec interrupt from device2 should be received.

Simply, Delay between interrupts of the same device is 10msec and delay between the devices is 5mesc.

How to implement this in kernel?

Regards,

ラベル(3)
0 件の賞賛
返信
0 返答(返信)