Surround view Application support for iMX6QP(Linux)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Surround view Application support for iMX6QP(Linux)

3,749件の閲覧回数
balasubramaniyam
Contributor II

Hi,

I am using Linux imx-4.9.11 release and Yocto Morty build  for iMX6QP.

How to add the support for "3D Surround view application" package in yocto for iMX6QP

I tried to build the surround view application in the iMX6QP device, but I got the segmentation fault while executing surround-view-3D_1.1_beta binaries.

NOTE:

Hoping for a better guidance.

 

Regards,

Bala

ラベル(2)
0 件の賞賛
返信
6 返答(返信)

3,382件の閲覧回数
kunyulei
Contributor I

I can run the demo correctly with INPUT=image.

But when I using the dumping image from my car, it can find the Contours correctly, but with a wrong grid output...

I am sure my template is right.

Could you please give some advice?

0 件の賞賛
返信

3,382件の閲覧回数
kunyulei
Contributor I

and I find if increase start_angle, it will segment fault...

<grid>

<angles>60</angles>

        <start_angle>4</start_angle>

<nop_z>30</nop_z>

<step_x>0.2</step_x>

<radius>1.7</radius>

</grid>

0 件の賞賛
返信

3,383件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Are you follow the build command in SVARM.pdf to build the BSP? The verified images in the document mentioned is L4.1.15. Please try to use L4.1.15 BSP.

0 件の賞賛
返信

3,383件の閲覧回数
balasubramaniyam
Contributor II

I tried both L4.1.15 BSP and L4.9.11 BSP package. Both got the same segmentation fault.

0 件の賞賛
返信

3,383件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

could you tell me the steps? so I can try to reproduce the problem on my side.

0 件の賞賛
返信

3,383件の閲覧回数
balasubramaniyam
Contributor II

Followed section "3. Building applications from sources" from SVARM.pdf to build the image.

After application built without any error, executing SV3D capturing binariesfrom the following path /Tools/CamCapture/capturing and I got the segmented failed error while running the SV3D capturing bianries.

Note:

  • I added some of the required packages in rootfs to built the SV3D application
0 件の賞賛
返信