Supporting HID in u-boot for IMX6UL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Supporting HID in u-boot for IMX6UL

1,401件の閲覧回数
ethanyang
Contributor II

Hi,

We're using imx_v2015.04_3.14.52_1.1.0_ga based u-boot.

We tried to build one utilizing the imx_udc driver, but encountered some random hang issue.

Is there sample code of HID driver in u-boot for imx6ul?

Regards,

Ethan

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,273件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ethan

may be useful to check attached bare metal usb mouse example from

sdk (full sdk may be obtained creating service request), please refer to pdf

document Chapter 34 Configuring the USB Host Controller Driver

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,273件の閲覧回数
ethanyang
Contributor II

Hi Igor,

Thanks for providing the example.

We found that the root cause is that we violated the usage of the USB controller, which is described in 54.4.5.1.1, IMX6UL RM:

Endpoint Capabilities/CharacteristicsThis DWord specifies static information about the endpoint, in other words, this information does not change over the lifetime of the endpoint. Device Controller software should not attempt to modify this information while the corresponding endpoint is enabled.

Regards,

Ethan

0 件の賞賛
返信