Suggestion over eink kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Suggestion over eink kit

1,947 Views
FrancescoFrassi
Contributor I

Hi all,

I would like to make an eink reader running Linux, with a good eink screen (I like so much the Pearl). What do you suggest?

 

 

Thanks in advance,

Frafra

Tags (1)
0 Kudos
Reply
2 Replies

1,726 Views
DannyNold
Contributor I

The i.MX50 Evaluation Kit with the E Ink add-on board would be a good way to get started.  The i.MX50 includes an integrated EPD (Electrophoretic Display) Controller, the EPDC, which accelerates the process of driving framebuffer data to the E Ink display.  The Pearl panel is supported using that board and configuration.

 

Thanks,

Danny

0 Kudos
Reply

1,726 Views
sammoser
Contributor I

Does the I.MX50 Evalutation Kit with the MX50EBOOKDC1 support partial updating of the screen (changing certain pixels without refreshing the whole display)?

Thanks!

0 Kudos
Reply