Spread Spectrum Clock for Ethernet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Spread Spectrum Clock for Ethernet

2,485 Views
kamil_zorychta
Contributor I

Hello,

Our platform based on I.MX6ull (Variscite DART 6ULL) with enabled 1 Ethernet port (of 2).

We would like to certificate our product, but we have got an EMC Ethernet issue.

During EMC tests we have observed 50MHz peak and its harmonics.

The disruption disappear when Ethernet went down (ifconfig eth0 down).

Is it possible to enable spread clock to Ethernet?

Best regards,

Kamil Zorychta

Labels (1)
0 Kudos
Reply
2 Replies

2,403 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kamil

>Is it possible to enable spread clock to Ethernet?

sorry not possible as only PLL2 has spread spectrum, ENET

PLL6 has not such functionality, this is described in Chapter 18
Clock Controller Module (CCM)

i.MX 6ULL Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,403 Views
kamil_zorychta
Contributor I

Hi Igor,

Thanks for answer.

So we will focus on pin configuration to smooth signals edges. It may help.

Best regards,

Kamil

0 Kudos
Reply