Spread Spectrum Clock for Ethernet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Spread Spectrum Clock for Ethernet

2,475件の閲覧回数
kamil_zorychta
Contributor I

Hello,

Our platform based on I.MX6ull (Variscite DART 6ULL) with enabled 1 Ethernet port (of 2).

We would like to certificate our product, but we have got an EMC Ethernet issue.

During EMC tests we have observed 50MHz peak and its harmonics.

The disruption disappear when Ethernet went down (ifconfig eth0 down).

Is it possible to enable spread clock to Ethernet?

Best regards,

Kamil Zorychta

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,393件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kamil

>Is it possible to enable spread clock to Ethernet?

sorry not possible as only PLL2 has spread spectrum, ENET

PLL6 has not such functionality, this is described in Chapter 18
Clock Controller Module (CCM)

i.MX 6ULL Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,393件の閲覧回数
kamil_zorychta
Contributor I

Hi Igor,

Thanks for answer.

So we will focus on pin configuration to smooth signals edges. It may help.

Best regards,

Kamil

0 件の賞賛
返信