Speed of Flash Interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Speed of Flash Interface

3,421 次查看
vinoth_ta
Contributor I

Hello, I have a been looking a solution to provide highest possible NAND Flash interface. imax8m itself having limitation to support TLC etc. 

From the application processors manual,

eMMC  => DDR mode can support up to 400 Mbytes/sec whereas raw NAND can support up to 200 Mbytes/sec. 

Looks like eMMC is faster than raw NAND. 

I am not clear on the ECC etc. Which interface(eMMC or raw NAND) will be having better throughput?

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

3,347 次查看
art
NXP Employee
NXP Employee

Yes, you are right, the SD/eMMC interface of the i.MX8M processor is faster than the Raw NAND interface.

For SD/eMMC devices, all ECC and other required processing is perfomed within the device, so, there are no special features required from the processor.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

3,347 次查看
vinoth_ta
Contributor I

Hi Artur,

Thanks for your information.

Is there any application note explain about these information.

I am interested to know the throughput of raw NAND or eMMC. I would need

to select the device which is having better throughput.

Regards,

Vinoth TA

0 项奖励
回复

3,347 次查看
art
NXP Employee
NXP Employee

There is no separate Application Note document for that. Please refer to the numbers, given in the Data Sheet document.

Best Regards,

Artur

0 项奖励
回复